Municipal wastewater refers to the contents of sewer systems. It can be made up of both sanitary sewage and stormwater, and can contain suspended solids, disease-causing pathogens, decaying organic wastes, nutrients and over 200 identified chemicals from industries, institutions, households and other sources. Municipal wastewater is released to lakes, rivers and oceans and it must be cleaned before allowing any effluent to enter communal waters. Most countries, municipalities and communities have laws regulating effluents.

 

A treatment plant should remove any potentially harmful material from the wastewater. The nature of the material and the methods used to remove it often determine its classification. Several steps are required to carry out the removal in wastewater.

 

With its extensive product basket Endress+Hauser has emerged as the only supplier able to meet all the instrumentation needs of today's wastewater treatment facilities.

 

For more information please click on une of the following plant steps  

                             WATER TREATMENT                       

                         SLUDGE MANAGEMENT                         

Public Channel Network

Static Pre-Thickener
Storm Water Basin Anaerobic Digester
Pump Station Secondary Thickener
Bar Screen Chamber Filter Press
Grease & Grit Removal Centrifuge
Primary Settling Tank Belt Filter Press
Aeration Basin  
Secondary Clarifier  
Denitrification Basin  

Sand Bed Filter

 

UV-Disinfection

 
Effluent Line (Basic Discharge)