Understanding critical water parameters
How do Life Science analysis instruments, pressure transmitters and more impact current Good Manufacturing Practice (cGMP) compliance?
By Bethany Silva, Life Sciences Industry Marketing Manager at Endress+Hauser
In pharmaceutical and bioprocessing settings, water is a regulated input that directly affects patient safety, batch consistency and audit results. Water quality, whether as Purified Water (PW), Water for Injection (WFI), RO/DI feedwater or clean steam, influences upstream processes, downstream purification, CIP/SIP and final rinse quality.
Regulators, including the FDA, EMA, PMDA and WHO, require continuous control of water-system parameters as defined in USP, EP, JP and ASME BPE. As expectations increase and systems grow more complex, maintaining stable control of conductivity, Total Organic Carbon (TOC) and pressure are essential to keeping utilities in a validated state. Modern life science analysis instruments, pressure transmitters and more make this level of monitoring and control achievable.
What are the critical parameters in pharma water systems?
Below are three parameters that may require continuous regulatory oversight, along with their significance.
1. Conductivity
What it measures: Ionic purity in PW and WFI
Why it matters: Early detection of contamination; identifies RO membrane failure or resin exhaustion; confirms loop balance and sanitization effectiveness
2. TOC
What it measures: Organic contaminants that fuel microbial growth
Why it matters: Prevents biofilm formation and endotoxin risk; ensures final water meets organic load limits
3. Pressure
What it measures: Hydraulic stability of recirculating water systems
Why it matters: Maintains consistent flow velocity; protects pumps and thermal system performance; ensures proper conditions in hot WFI and clean steam loops
Deviations in these three parameters increase compliance risk, microbial risk and operational instability, making real-time monitoring essential. However, there are other important measurement parameters, including flow and temperature that can also be monitored.
Why does digitalization matter for modern cGMP utilities?
Current cGMP expectations go beyond measurement accuracy. Regulators require traceable, tamper-proof, digital data that demonstrate continuous control. As a result, Life Science utilities increasingly rely on:
Digital Memosens liquid analysis devices:
Contactless, contamination proof signal transmission
Full sensor traceability with calibration history, exposure data, serial identity
Predictive diagnostics for proactive maintenance
Plug and play sensor exchange without user induced variability
Heartbeat Technology:
Continuous internal self-monitoring
Compliant, in process verification without removing sensors
Automated audit-ready verification reports
Reduces calibration burden and supports risk-based lifecycle management
Together, these digital technologies support 21 CFR 11 compliance, reduce manual documentation and keep systems inspection-ready at all times.
How can standardizing improve clean utility reliability?
Many facilities may encounter inconsistent device types, documentation gaps and redundant CQV workloads. Standardizing instrumentation across PW, WFI and clean-steam systems provides:
Harmonized SOPs and qualification templates
Faster commissioning and requalification
Reduced operator training requirements
More predictable calibration cycles
Stronger audit defense through consistent verification behavior
Lower lifecycle and maintenance costs
The result is a clean-utility platform that is easier to manage, defend during audits and scale from laboratory to pilot to commercial operations.
Liquid analysis instrumentation for pharma water systems
Conductivity (ionic contamination control): Digital conductivity sensor Memosens CLS16E - hygienic Memosens conductivity sensor for PW/WFI; high accuracy under thermal stress; fully CIP/SIP compatible.
TOC (organic load monitoring): Low-range TOC analyzer CA79 - low-range TOC analyzers using UV oxidation and differential conductivity; rapid response times ideal for online PW/WFI monitoring.
Pressure instrumentation for pharma water systems
Hydraulic loop stability: Cerabar PMP43 - ASME BPE compliant Cerabar transmitter for hot WFI, recirculation loops and clean steam applications.
Flow measurement for pharma water systems
Distribution control & utility measurement: Proline Promass P 100 - Coriolis flowmeter designed for applications in sterile environments; ideal for water distribution skids, WFI recirculation and dosing; Proline Promass P 300 - Coriolis flowmeter dedicated to biotech applications requiring highest compliance with guidelines and regulations, high flexibility in terms of operation and system integration with access from one side, remote display and improved connectivity options.
Temperature measurement for pharma water systems
Thermal mapping & SIP assurance: TrustSens TM372 - self-calibrating hygienic temperature sensor delivering automatic inline calibration events; iTEMP TMT36 - reliable, long-lasting, single-channel IO-Link temperature head transmitter with a form B connection head.
Digitalizing pharma water systems
Transmitters & digital integration: Liquiline M CM42B, stainless hygienic version - preferred Liquiline transmitter for Life Science utilities; DIN rail mount installation option; fully compatible with Memosens sensors and digital diagnostic workflows.
Keeping critical water parameters under control
Pharmaceutical utilities are only as reliable as the instrumentation used to monitor them. Due to stringent purity requirements, high uptime expectations and increased audit scrutiny, manufacturers rely on stable, digital and compliant measurement technologies.
By focusing on the three most critical water parameters—conductivity, TOC and pressure—and adopting a holistic platform built around:
Manufacturers can achieve stronger compliance, improved operational reliability and a continuous state of cGMP control.
To learn more about Endress+Hauser or to speak with an expert, click here.
Frequently asked questions
What is the purpose of cGMPs?
The purpose of current Good Manufacturing Practices (cGMPs) is to ensure that pharmaceutical and biopharmaceutical products are consistently manufactured, controlled and documented in a way that protects patient safety, product quality and data integrity.
What is cGMP certified?
cGMP compliance means that a manufacturer, facility or process has been evaluated and found to operate in accordance with current Good Manufacturing Practice regulations during a regulatory inspection or audit.
What does GMP certified mean?
It means a facility has passed regulatory inspection and demonstrated robust control over equipment, documentation and processes that impact product quality and patient safety.
What does GMP compliant mean?
GMP compliant means the operation follows GMP principles such as validated equipment, change control, SOPs and data integrity, even without formal certification.