Here’s why you should consider a Coriolis flowmeter in your industrial processes
Taking a close look at how Coriolis flowmeters work, their advantages and more
By Lauton Rushford, Flow Product Marketing Manager at Endress+Hauser
In industrial environments, choosing the right flow measurement device can significantly impact product quality, process efficiency and operational safety. Enter the Coriolis flowmeter, which uses the Coriolis effect to deliver accurate, multivariable data in real time.
What is the Coriolis effect?
The Coriolis effect is a physical phenomenon that occurs when a mass moves within a rotating or oscillating system. As the mass flows through a vibrating tube, it experiences a deflection due to inertia. This twist or phase shift is what Coriolis flowmeters detect and measure. The greater the flow rate, the greater the deflection, allowing the flowmeter to calculate mass flow with high precision.
How do Coriolis flowmeters work in industrial applications?
Coriolis flowmeters operate by vibrating flow tubes and measuring the phase shift caused by fluid movement. This shift, a result of the Coriolis effect, is directly proportional to the mass flow rate. Sensors also detect changes in resonant frequency to determine fluid density, while integrated temperature probes provide thermal data. These measurements allow for real-time monitoring of fluid properties, even in complex or multiphase flows.
What are the main advantages of using a Coriolis flowmeter?
Coriolis flowmeters offer several key benefits:
Direct mass flow measurement without the need for conversion from volumetric flow
Multivariable sensing including mass flow, density, temperature and viscosity
High accuracy and repeatability, even in challenging conditions
No moving parts, reducing maintenance and increasing reliability
Application-specific designs; Endress+Hauser offers 17 sensor types tailored to industry needs
Which instruments are best for flow rate and mass flow rate?
Innovations such as Proline Promass Q, which compensates for entrained air using multi-frequency oscillation, and Proline Promass U, a single-use flowmeter for sterile pharmaceutical environments, further expand the technology’s versatility. Proline Promass I adds viscosity monitoring and trending for Newtonian and non-Newtonian fluids, while the Proline Promass K 10 introduces IO-Link connectivity for cost-effective digital integration.
What to consider when installing a Coriolis mass flowmeter?
Proper installation is critical to ensure optimal performance. Consider the following:
Horizontal or vertical placement affects how fluids behave inside the flowmeter
External vibrations can interfere with internal oscillation; use dampeners or brackets
Ensure the flowmeter’s materials match operating conditions
Confirm compatibility with control systems (EtherNet/IP, IO-Link, etc.)
Use factory-calibrated sensors and enable Heartbeat Technology for real-time verification
Unlike other flowmeters, Coriolis devices typically do not require any straight pipe run, but ensuring the tubes are fully filled during operation is essential.
Where can I find professional flowmeter calibration service?
Endress+Hauser provides comprehensive calibration and verification services through its global network of service centers and on-site support teams. Whether you need ISO 17025-accredited calibration, traceable certificates or in-situ verification using Heartbeat Technology, Endress+Hauser ensures your Coriolis flowmeters maintain peak accuracy and compliance.
You can schedule calibration at one of Endress+Hauser’s accredited facilities or request mobile calibration services for minimal downtime. Visit Endress+Hauser’s Service Portal to find local experts and book your calibration appointment.
Conclusion
Coriolis flowmeters are transforming how industries measure and manage fluid flow. By leveraging the Coriolis effect, these devices deliver unmatched precision and adaptability. Whether you're measuring crude oil, dairy products or pharmaceutical ingredients, Coriolis flowmeters offer the accuracy, reliability and insight needed to optimize modern industrial processes.
Endress+Hauser’s Coriolis flowmeter portfolio is built to support all industries.