Title

Try searching by key words, order- or product code or serial number e.g. “CM442” or “Technical information”
Enter at least 2 characters to start the search.

How do I choose the right flow switch or sensor for my industrial application?

Electromagnetic flowmeters, continuous diagnostics and condition-based monitoring help maintain measurement integrity in harsh Oil & Gas environments

Publication date: 03/31/2026

By Cesar Adan Martinez Castillo, Oil & Gas Industry Marketing Manager, Endress+Hauser USA

Build‑up inside pipelines and flowmeters is one of the most persistent operational challenges in modern Oil & Gas environments. Across upstream production, midstream transport and downstream processing, deposits such as paraffin, asphaltenes, scaling minerals, magnetite and corrosion byproducts can accumulate gradually inside flowmeters.

Long before these deposits cause visible flow disruption, they distort the electromagnetic field, reduce accuracy and increase the likelihood of unplanned intervention. Maintaining stable measurement therefore requires not just a rugged meter, but continuous visibility into what is happening inside it. 

The Proline Promag P electromagnetic flowmeter, purpose‑built for chemically aggressive and high‑temperature service, delivers that visibility through Heartbeat Technology. With permanent diagnostics, in‑situ verification and advanced build‑up monitoring, Proline Promag P allows Oil & Gas operators to detect coating formation early, understand how it progresses and act at the right moment to protect flow assurance.

Detect signs of flow restriction in harsh production streams

Paraffin films, brine‑based scale, corrosion layers or magnetite deposits typically begin forming in thin, uniform layers that may go unnoticed until measurement drift or pressure changes indicate a problem.

Heartbeat Technology continuously analyzes signal variation within the Proline Promag P measuring tube and translates these subtle changes into a quantifiable build‑up index. This gives operators a clear indicator of whether deposits are forming, how quickly they are developing and whether they are affecting measurement stability. 

This early insight allows production teams to time cleaning and chemical treatment based on actual coating behavior rather than fixed intervals. As a result, maintenance becomes proactive rather than reactive, supporting stronger flow assurance and reducing the risk of unexpected downtime.

Support separation with measurement in changing conditions

Separation systems—whether two‑phase, three‑phase or test separators—handle fluids with shifting compositions and varying conductivity. Produced water content, salinity, trace solids and temperature changes all influence process behavior, and these dynamic conditions make build‑up a realistic and recurring threat. 

Proline Promag P’s chemically resistant lining and stable electromagnetic measurement principle allow it to handle fluids with variable conductivity and suspended contaminants without compromising accuracy. 

Heartbeat Technology’s build‑up index equips production engineers with continuous insight into internal fouling, especially in conditions where iron‑based compounds, scaling minerals or emulsified hydrocarbons adhere to the sensor. By monitoring the onset of these deposits, Proline Promag P helps maintain consistent measurement during slugs, emulsion shifts and operational fluctuations common in separation trains. 

Improving desalting performance

Desalting units introduce challenges that traditional flowmeters struggle to detect. High‑conductivity fluids, magnetite formation, electrostatic fields, chemical additives and fluctuating temperatures can all impact measurements. Proline Promag P meets these demands with its robust materials of construction and built‑in diagnostics. 

Heartbeat Technology offers two layers of protection in desalting environments: 

  • Build‑up detection, which identifies conductive films such as magnetite or corrosion solids before they distort the electromagnetic field

  • Heartbeat Sensor Integrity, which detects magnetic interference from high‑current equipment or process conditions that could influence signal quality

Together, these functions give operators a clear picture of when the flowmeter is being affected by deposit formation or electrical interference, critical information for maintaining reliable measurement in the desalter vessel or downstream wash‑water systems.

Enhancing reinjection and discharge reliability

Reinjection systems are prone to scaling and iron‑oxide deposition due to high salinity, temperature shifts and chemical carryover. These deposits reduce cross‑sectional area, increase friction and can impair injectivity if left unmonitored. 

Proline Promag P with Heartbeat Technology gives reinjection teams a quantifiable trend showing how build-up forms and stabilizes over time. This supports more effective planning of cleaning, chemical treatment or acidizing and helps avoid unnecessary interventions. 

Because reinjection often occurs in remote or unmanned locations, the ability to verify flowmeter condition without removing the device from service adds significant operational value. 

Strengthen measurement confidence in hydrocarbon processing

Across pipelines, separators, dehydration units, produced‑water skids and chemical‑injection systems, measurement reliability depends on both sensor durability and diagnostic transparency. Proline Promag P combines rugged construction with extensive internal monitoring to ensure confidence in any environment where conductive, corrosive or fouling-prone fluids are present. 

With real‑time diagnostic data accessible through the device, automation tools or control‑room interfaces, operators can maintain full visibility into coating progression, sensor integrity and overall meter health. This enables efficient troubleshooting, reduces maintenance variability and helps ensure that measurement remains dependable even as operating conditions shift.

Flow assurance in Oil & Gas increasingly depends on having reliable, self‑monitoring instrumentation capable of detecting internal changes before they become operational problems. Proline Promag P with Heartbeat Technology provides visibility.

By combining rugged engineering with continuous diagnostics, in‑situ verification and quantifiable build‑up detection, it supports a transition from scheduled maintenance to condition‑based strategies that protect uptime, reduce cost and preserve measurement accuracy in demanding hydrocarbon environments.

Proline Promag P offers deep insight into the factors that determine whether a measurement remains reliable. For Oil & Gas operators looking to strengthen process stability, gain earlier visibility into fouling and minimize unplanned intervention, Heartbeat Technology delivers a clear advantage.

To speak with an Endress+Hauser expert or to learn more about electromagnetic flowmeters, click here.

Read more about similar topics:

Press list

Receive the next press releases and news directly in your mailbox. Stay up to date by subscribing to the Endress+Hauser press list.

Endress+Hauser press list

Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

Select the topics you are interested in:  *
Select the industries you are interested in: *

Personal Data


Fields marked with * are required. You will receive an email with a confirmation of your subscription. The information enlisted is voluntary and your data will only be used for personalizing your newsletters and not be passed onto any third party. For statistical reasons we will perform anonymous link tracking.