How do point level switches keep chemical plants safe, compliant and running?
Liquiphant devices for tank overfill protection
By Keith Riley, Level+Pressure Product Marketing Manager at Endress+Hauser
As a chemical manufacturer, safety is always the first priority — protecting people, facilities and surrounding communities. When an overfill occurs, it’s an immediate safety hazard, a potential shutdown, environmental exposure, lost production and pressure on P&L. That’s why best‑practice tank overfill protection is a critical safeguard for safe, reliable and compliant operations.
For these reasons, many facilities can rely on point level switches, especially vibronic technology like Endress+Hauser’s Liquiphant, to create a reliable line of defense. These instruments are designed for harsh conditions, require minimal maintenance and deliver the dependability needed to keep chemical plants running efficiently.
How do point level sensors work?
Point level sensors detect when a liquid reaches a specific level, usually a high or low limit. Vibronic switches, like Endress+Hauser’s Liquiphant family, use a vibrating fork to sense contact with liquid. The presence of media dampens the fork’s vibration frequency, triggering a precise switch signal.
Because this principle is immune to foam, turbulence, viscosity changes, coating or density shifts, it remains stable even when processes don't. This is critical in plants where feedstock quality varies, multiphase mixtures occur or tank behaviors shift throughout the day. Devices such as Liquiphant FTL41, FTL51B, FTL62 and FTL64 are built specifically to handle these unpredictable realities.
For hazardous, corrosive or high‑temperature media, advanced models like Liquiphant FTL62, FTL64 and FTL80/81 FailSafe offer rugged construction and specialized materials to withstand aggressive conditions without drift or degradation. Liquiphant FTL62 is engineered for aggressive chemical media, with coatings such as ECTFE, PFA and enamel, while Liquiphant FTL64 handles temperatures up to 536°F.
What makes up a complete overfill protection system?
A complete overfill protection system should be designed to be simple to maintain, predictable in operation, compliant with safety requirements and difficult to bypass. Each element, from the level switch to the logic solver and final control element, should work together as a dependable, easy‑to‑manage protection layer that supports safe, consistent and audit‑ready operation.
A complete system includes:
A Liquiphant point level switch serving as the limit detector
A logic solver or safety controller evaluating the signal
A final control element (pump, valve, shutdown command)
Proof testing procedures that are easy for operations to perform
Diagnostics that support predictive maintenance
Many models — including Liquiphant FTL51B, FTL63, FTL71 and FTL85 — are SIL2/SIL3 capable and designed according to IEC 61508 to meet modern functional safety expectations.
This combination reduces the likelihood of spurious trips and dangerous failures, both of which directly affect uptime and operational performance.
Why do point level switches work for overfill protection?
When it comes to tank overfill protection, point level switches bring advantages that map directly back to a chemical plant manager’s needs.
Liquiphant excels because:
It offers ease of installation with minimal commissioning effort
It is unaffected by foam, buildup, bubbles or changing product properties, ensuring a stable SIL-rated alarm
It requires no calibration, which reduces the burden on teams
It simplifies compliance through guided proof tests and automatic verification reports
Advanced devices like Liquiphant FTL51B, include Heartbeat Technology, enabling in-situ health verification, real-time predictive maintenance and “at-a-glance” diagnostic checks that allow teams to spot corrosion or coating before it reaches the failure stage.
Can overfill protection prevent environmental hazards?
Preventing environmental hazards aligns directly with a manufacturer's responsibility for regulatory compliance and environmental performance. An effective overfill protection system prevents spills that can contaminate groundwater, soil or waterways.
Devices like Liquiphant help ensure tanks never exceed their safe limits, enabling compliance with WHG, EPA and industry-specific regulations. Since many Liquiphant models offer guided proof testing and automated documentation, compliance audits become more efficient and transparent. Manufacturers can also avoid environmental exposure, community impact, cleanup costs and the operational damage of incident investigations.
What are common apps of point level switches in industry?
Tank overfill protection is only one application and that’s part of why plant managers from various industries value vibronic switches. Their versatility reduces SKUs, training and spare parts complexity.
Holistically, Liquiphant point level switches protect:
Corrosive chemical tanks, reactors, boilers and storage tanks
Hazardous transfer operations
Flammable fuel storage
High temperature solvent processing
Pump run-dry conditions
Water and wastewater sumps
Rugged FailSafe models like Liquiphant FTL80/81 cover extreme chemical, temperature and safety requirements.
New-generation replacements like Liquiphant FTL51B, FTL62 and FTL64 offer digital enhancements and more efficient proof testing.
Liquiphant models at a glance
To support manufacturer's planning, here is a compact list of Liquiphant devices:
Standard & compact models: Liquiphant FTL41
General purpose/modernized models: Liquiphant FTL51B
Chemical/hazardous/corrosive applications: Liquiphant FTL62 (aggressive media), FTL64 (high temperature)
FailSafe/SIL3 applications: Liquiphant FTL80, FTL81, FTL85
This lineup ensures standardization across facilities while still matching each process requirement.
Built for chemical manufacturers who need certainty
Chemical manufacturers demand clear visibility, predictable performance and equipment that supports — not complicates — operational strategy. Tank overfill protection built around Liquiphant point level switches provide confidence that tanks will not exceed safe levels, that safety loops remain compliant and that plants stay online.
With proven-measurement principles, SIL-rated design, digital diagnostics and rugged construction, Liquiphant delivers what plant managers value most: reliability, simplicity and long-term operational stability.
To learn more about Endress+Hauser or to speak with an expert, click here.