How to connect Bluetooth® instrumentation with the IIoT
Your connectivity guide in three simple steps
Article01/05/2026
In brief
Industrial environments rely heavily on cables and interfaces for device connectivity and setup, often requiring multiple dongles for different protocols.
The use of dongles has long been standard in industry, similar to the variety of adapters and cables common in everyday life.
Wireless communication has gradually gained acceptance, starting with limited standards and proprietary protocols, later moving toward open solutions like WirelessHART.
Bluetooth® introduces a tipping point by enabling seamless integration with the cloud and driving practical digitalization for smarter plants.
Table of contentsTable of contents
The era of dongles in automation is nearing its end
In industrial automation, accessing device configurations has traditionally required multiple adapters and interfaces. Typical scenarios include requests for RS-485 adapters, HART interfaces, Ethernet cables, or even tools for 4–20 mA signals. This complexity often results in delays and inefficiencies.
Such challenges are common across manufacturers. Depending on the protocol and device type, a specific interface is often necessary to retrieve parameters or perform diagnostics. While solutions that completely eliminate dongles are still in development, wireless technologies already offer fast access to devices.
Protocols like WirelessHART have gained popularity, yet their adoption remains limited compared to traditional 4–20 mA connections, despite offering remote access to diagnostic and configuration data. This raises an important question: how can wireless be implemented effectively in smaller applications?
The answer lies in devices equipped with an additional protocol - Bluetooth®. This technology enables quick and easy access to device data while maintaining the standard 4–20 mA signal for controller connectivity.
Simplifying access with Bluetooth®-enabled field devices
Replacing a device with a similar model is far easier than switching to one with a different protocol. However, modernization is inevitable, and during this transition, accessing diagnostic and configuration data remains critical.
New field devices now offer dual communication capabilities. They maintain traditional 4–20 mA integration while providing configuration and diagnostic access via a mobile application on a smartphone or tablet. This local connectivity requires the field engineer to be physically near the device.
For smaller applications, another challenge arises: how to remotely access diagnostic data collected through Bluetooth® and integrate it into broader systems? The solution is here—Bluetooth® devices can now transmit diagnostics to the cloud using IIoT services. Remote applications can also incorporate primary and secondary process variables into existing systems.
Implementation is straightforward and can be achieved in three steps, enabling organizations to begin their IIoT journey by thinking big but starting small.
How to make your plant digital in three steps
Organizations seeking to leverage Bluetooth® technology in existing plants or new applications can achieve this through three straightforward steps. Following these steps ensures that all relevant data is securely available in the cloud, ready for integration and analysis.
Step 1 – Bluetooth®-enabled devices
Modern field devices increasingly support Bluetooth® communication, simplifying connectivity and configuration. For example, replacing a temperature transmitter can now involve selecting a model that combines Bluetooth® with traditional 4–20 mA or other technologies. For new applications requiring remote monitoring, Bluetooth® devices provide an efficient way to collect data locally and transmit it wirelessly to an edge device.
Step 2 – FieldEdge
Once a Bluetooth®-enabled device is installed, its data can be collected and sent to a cloud solution via an edge device, such as the Endress+Hauser FieldEdge SGC200. The FieldEdge SGC200, powered locally, connects to up to five Endress+Hauser devices within a 20-meter range and transmits primary process values (PV), secondary process values (SV), and NAMUR NE107 status information. Communication with the cloud occurs via 3G or 4G using a built-in global SIM card, with encryption ensuring maximum security. Importantly, this connection is one-way: the edge device reads data cyclically, preventing any remote control of field devices.
Step 3 – Cloud solution and API
To complete the setup, a cloud service subscription is required. Offerings such as Netilionprovide a comprehensive IIoT ecosystem, including the edge device, cloud infrastructure, and an Application Programming Interface (API). The cloud platform consolidates all field data in a secure environment. Netilion Connect uses a REST/JSON API, enabling straightforward data consumption and integration into control systems, SCADA, or custom applications. This approach offers flexibility and scalability, allowing organizations to leverage field data securely and efficiently.
Examples of applications
Implementing Bluetooth® technology in small-scale applications is a practical first step toward digitalization. Below are several use cases that illustrate its potential when combined with IIoT cloud services:
Remote diagnostic monitoring
Critical assets can be monitored remotely using Bluetooth® devices. This approach provides NE107 device status information, enabling health monitoring that reduces unscheduled downtime and supports a shift from corrective to predictive maintenance through historical diagnostics.
By using Endress+Hauser Bluetooth® devices together with FieldEdge, simple level monitoring becomes accessible from any location. Data and diagnostics can be integrated into existing systems via Netilion Connect. For inventory management, additional solutions such as Netilion Inventory or SupplyCare offer enhanced functionality.
For smaller installations involving level, flow, or temperature monitoring, Bluetooth® devices combined with FieldEdge SGC200 and API integration provide a flexible, cost-effective solution. Minimal infrastructure is required to collect and transmit data securely, ensuring accessibility wherever needed.
Bluetooth®-enabled devices offer a simple and effective way to transfer critical data to the cloud. Combined with edge devices and API-based solutions, this approach ensures secure data collection and provides the flexibility to integrate information into any system of choice.
Netilion is an award-winning IIoT ecosystem, designed for industrial processes. It connects the physical and digital worlds to send valuable information from the field to you anywhere at any time.
This session will dive into the critical role of Safety Instrumented Systems and Safety Integrity Levels in chemical processes, helping you understand best practices for risk reduction and compliance.
At the end of the course you will know about the features of the PROFINET technology and the PA profiles, network design of 100BaseTX and Ethernet-APL.