Title

Try searching by key words, order- or product code or serial number e.g. “CM442” or “Technical information”
Enter at least 2 characters to start the search.

Advantages of ultrasonic flow measurement in Chemical

Considerations for choosing an ultrasonic flowmeter (clamp-on) in the Chemical industry

Endress+Hauser’s ultrasonic clamp-on flow measurement technologies provide a practical way to add or improve flow visibility in chemical plants without opening the pipe. Because the sensors mount externally, there are no wetted parts and no additional leak paths, which can be advantageous for corrosive, hazardous or difficult-to-handle fluids. For chemical apps, two choices are Proline Prosonic Flow W 400 for standard liquid services and Proline Prosonic Flow P 500 for demanding requirements.

Considerations for choosing an ultrasonic flowmeter (clamp-on) in the chemical industry ©Endress+Hauser

How clamp-on ultrasonic flowmeters work and their advantages

  • Non-intrusive clamp-on installation (no wetted parts, no new leak paths)

  • Can be applied where opening the pipe is costly or undesirable (retrofit-friendly)

  • Free pipe cross-section (no pressure loss introduced by the flowmeter)

  • Supports common chemical use cases: utilities, transfer lines, verification and troubleshooting (application dependent)

  • Improved usability on existing piping using configuration support such as flow disturbance compensation and diagnostics (where available)

Flowmeter challenges in the Chemical industry

In chemical service, adding flow measurement can be challenging when the process fluid is corrosive, hazardous, abrasive or when a shutdown is difficult to schedule. Traditional inline flowmeters often require pipe cutting, hot work permits, drain-and vent procedures and new sealing surfaces, driving cost, risk and downtime.

At the same time, chemical plants still need dependable flow data for mass balance, utility management, transfer verification and process control. Existing piping layouts may also limit available straight runs (valves, elbows, reducers) and make it challenging to achieve stable readings with some technologies, especially when a fast, low-disruption retrofit is required.

What to consider when choosing an ultrasonic flowmeter

Clamp-on ultrasonic flowmeters use the transit-time principle: ultrasonic signals travel with and against the flow, and the resulting travel-time difference is proportional to flow velocity. With externally mounted sensors, measurement is non-intrusive, supporting installation without opening the line, keeping the pipe cross section free and adding no pressure loss.

For chemical plants, Endress+Hauser offers two clamp-on ultrasonic flowmeter technologies to match typical requirements: Proline Prosonic Flow W 400 for many standard liquid services, and Proline Prosonic Flow P 500 for higher-demand applications such as elevated temperatures, hazardous area approvals and/or functional safety (SIL), depending on configuration.

Contact us

Are you interested in our offering? Would you like to discuss about your application?

Please let us know as detailed as possible how we can help you. That way we can get back to you with the best possible answer.