Title

Try searching by key words, order- or product code or serial number e.g. “CM442” or “Technical information”
Enter at least 2 characters to start the search.

Endress+Hauser unveils Picomag flowmeter for data centers, OEM applications in US market

Flow device primed for security in data center and OEM applications at various stages of the liquid cooling process 

Publication date: 03/09/2026

Endress+Hauser today announces a new OEM-configured variant of the Picomag electromagnetic flowmeter for the US market. Purpose-built for liquid cooling applications in data centers and OEM cooling systems, this version provides customers with a factory-configured option designed for environments where instrumentation without wireless connectivity is required.

Picomag is Endress+Hauser's compact electromagnetic flowmeter designed for accurate measurement of conductive fluids in small-diameter pipelines. It combines flow, temperature and conductivity measurement in a single device.

While the standard Picomag includes industry-leading Bluetooth® technology that meets rigorous global cybersecurity standards, many data centers and OEM partners operate under policies that prohibit wireless communication of any kind.

Purpose-built for high-security data center environments

The OEM variant meets this operational preference by offering a  Picomag model delivered with Bluetooth® deactivated from the factory, ensuring alignment with facility policies while maintaining all core Picomag performance capabilities. In this configuration, the device integrates seamlessly through IO‑Link or standard signal outputs — 4–20 mA current, pulse, switch or 2–10 V — offering a controlled starting point ideal for secure or regulated environments. 

"Data centers operate under some of the most demanding security expectations in the world,” said Nathan Hedrick, Product Marketing Group Manager at Endress+Hauser. “This OEM Picomag gives cooling system designers a compact, reliable and secure measurement option tailored for environments where wireless features are not permitted without compromising on the functionality our customers expect.” 

The OEM Picomag variant is designed to integrate seamlessly into standardized cooling skids, secondary distribution loops and rack‑level cooling modules. Key characteristics include: 

  • Factory‑delivered with wireless connectivity deactivated to meet strict facility requirements

  • Preconfigured display behavior, output settings and engineering units for consistent OEM deployment

  • Available in 1” and 2” sizes, ideal for compact rack or subsystem cooling circuits 

This version retains all Picomag’s hallmark advantages, including flow, temperature and conductivity measurement, a bright, auto‑rotating display, intuitive commissioning and built‑in diagnostic capabilities. 

"This addition strengthens our ability to support every stage of a data center facility's cooling architecture," said Lauton Rushford, Flow Product Marketing Manager at Endress+Hauser. "It ensures operators and OEMs can select instrumentation that aligns with their policies while benefitting from Picomag's proven performance and simplicity."

How does liquid cooling compare to traditional air cooling?

As data centers grow in density and power consumption, many operators are shifting from traditional air-cooling systems to liquid cooling architectures. Liquid cooling offers significantly greater heat‑removal efficiency, allowing facilities to manage higher thermal loads generated by modern CPUs and GPUs.  

While air cooling relies on large volumes of conditioned airflow, liquid cooling absorbs and transports heat far more effectively, supporting higher rack densities, reducing energy use and enabling more compact system designs. This shift is especially pronounced in AI, hyperscale and high‑performance computing environments where equipment demands exceed what air cooling alone can accommodate. 

Liquid cooling also supports more precise thermal management at the subsystem or rack level. This creates new measurement requirements for inline flow and temperature monitoring, which is where compact, secure devices like the OEM Picomag play a key role.  

What are the latest trends in data center optimization tech?

As data centers adopt increasingly complex liquid‑cooling architectures driven by high‑density GPU workloads, AI clusters and expanding global capacity, operators need compact, accurate measurement at more distributed points in the cooling network. 

The OEM Picomag complements Endress+Hauser’s broader flow portfolio, including Proline Promag W 300/500 (0xDN), enabling a complete, scalable measurement strategy spanning from large‑diameter primary loops to small‑diameter subsystem circuits. 

Stable water quality is also essential for maintaining liquid cooling efficiency. Complementary technologies such as inline liquid analysis (pH, conductivity, turbidity) help operators prevent scaling, corrosion and fouling, further supporting uptime and thermal stability. 

Endress+Hauser enables operators and OEM partners to build cooling systems that are efficient, scalable and aligned with their security and operational policies. 

To learn more about Endress+Hauser’s data center offerings, click here. To connect with an Endress+Hauser sales and service representative, click here.

Read more about similar topics:
  • Endress+Hauser press list

    Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

    Select the topics you are interested in:  *
    Select the industries you are interested in: *

    Personal Data


    Fields marked with * are required. You will receive an email with a confirmation of your subscription. The information enlisted is voluntary and your data will only be used for personalizing your newsletters and not be passed onto any third party. For statistical reasons we will perform anonymous link tracking.